Register ADC channel buffer.
int32_t adc_os_register_channel_buffer( struct adc_os_descriptor *const descr, const uint8_t channel, uint8_t *const convert_buffer, const uint16_t convert_buffer_length )
This function initializes the given ADC channel buffer descriptor.
Type: struct adc_os_descriptor Struct *const
An ADC descriptor to initialize
Type: const uint8_t
Channel number
Type: uint8_t *const
A buffer to keep converted values
Type: const uint16_t
The length of the buffer above
Type: int32_t
Initialization status.
Passed parameters were invalid or an ADC is already initialized
The initialization is completed successfully