In the Pulse Width Modulation (PWM) asynchronous driver, a callback function can be registered in the driver by the application and triggered when errors and one PWM period is done.
The user can change the period or duty cycle whenever PWM is running. The function pwm_set_parameters is used to configure these two parameters. Note that these are raw register values and the parameter duty_cycle means the period of first half during one cycle, which should be not beyond the total period value.
In addition, the user can also get multiple PWM channels output from different peripherals at the same time, which is implemented more flexible by the function pointers.
Initialize and deinitialize the driver and associated hardware
Hookup callback handlers on errors and one PWM period
Enable or disable the PWM related hardware
Run-time control of PWM duty-cycle and period
The PWM waveform duty value
The PWM waveform period value
The current driver doesn't support the features like recoverable, non-recoverable faults, dithering, and dead-time insertion.
The following shows a simple example of using the PWM. The PWM must have been initialized by pwm_init. This initialization will configure the operation of the related PWM hardware, such as input pins, period, and duty cycle.
/**
* Example of using PWM_0.
*/
void PWM_0_example(void)
{
pwm_set_parameters(&PWM_0, 10000, 5000);
pwm_enable(&PWM_0);
}
The peripheral which can perform waveform generation like frequency generation and pulse-width modulation, such as Timer/Counter.
The NVIC must be configured so that the peripheral interrupt requests are periodically serviced