Set the required layer size.
static int32_t lcd_set_size( uint8_t layer, int32_t x, int32_t y )
This function set the required layer size.
Type: uint8_t
Index of layer, 0 for base layer.
Type: int32_t
Physical X-position to be used to set up the layer size.
Type: int32_t
Physical Y-position to be used to set up the layer size.
Type: int32_t
Set status.