Reset the root hub port.
static void usb_h_rh_reset( struct usb_h_desc * drv, uint8_t port )
Type: struct usb_h_desc *
Pointer to the USB HCD driver
Type: uint8_t
Root hub port, ignored if there is only one port
Type: void