Set YUV framebuffer for the required layer.
static int32_t lcd_show_streams( uint8_t layer, void * fb1, void * fb2, void * fb3 )
This function set the YUV framebuffer pointer for the required layer.
Type: uint8_t
Index of layer.
Type: void *
Pointer to framebuffer of Y.
Type: void *
Pointer to framebuffer of U or UV, NULL if no used.
Type: void *
Pointer to framebuffer of V, NULL if no used.
Type: int32_t
Set status.