The serial peripheral interface (SPI) is a DMA serial communication interface.
The SPI Master DMA driver uses the DMA system to transfer data from a memory buffer to the SPI (Memory to Peripheral), and receive data from the SPI to a memory buffer (Peripheral to Memory). User must configure the DMA system driver accordingly. A callback is called when all the data is transfered or received, if it is registered via the spi_m_dma_register_callback function.
Refer SPI Drivers for more detailed SPI basics.
Initialize and deinitialize the driver and associated hardware
Register I/O descriptor
Enable or disable SPI master
Hookup callback handlers on read/write/transfer complete, or error events
Read/Write message to/from the slave
Select SPI DMA TX channel
Select SPI DMA RX channel
Select character size
Set SPI baudrate
Which clock source is used
After the SPI hardware initialization, the spi_m_dma_get_io_descriptor function is needed to register an I/O descriptor. Then use spi_m_dma_register_callback to register a callback function for the RX/TX/transfer, and enable SPI hardware complete. Then, control the slave select (SS) pin and start the read/write operation.
The slave select (SS) is not automatically inserted during read/write/transfer. The user must use an I/O to control the devices'SS.
When the DMA channel is only used for receiving data, the transfer channel must be enabled to send dummy data to the slave.
While read/write/transfer is in progress, the data buffer used must be kept unchanged.
The following shows a simple example of using the SPI master DMA. The SPI master must have been initialized by spi_m_dma_init. This initialization will configure the operation of the SPI master.
The example registers an I/O descriptor and enables the hardware. Then it registers a callback, and finally starts a writing operation.
/**
* Example of using SPI_0 to write "Hello World" using the I/O abstraction.
* Since the driver is asynchronous we need to use statically allocated memory for string
* because driver initiates transfer and then returns before the transmission is completed.
* Once transfer has been completed the tx_cb function will be called.
*/
static uint8_t example_SPI_0[12] = "Hello World!";
static void tx_complete_cb_SPI_0(struct _dma_resource *resource)
{
/* Transfer completed */
}
void SPI_0_example(void)
{
struct io_descriptor *io;
spi_m_dma_get_io_descriptor(&SPI_0, &io);
spi_m_dma_register_callback(&SPI_0, SPI_M_DMA_CB_TX_DONE, (FUNC_PTR)tx_complete_cb_SPI_0);
spi_m_dma_enable(&SPI_0);
/* Control the slave select (SS) pin */
//gpio_set_pin_level(SPI_0_SS, false);
io_write(io, example_SPI_0, 12);
}
The SPI master peripheral and its related I/O lines and clocks
The NVIC must be configured so that SPI interrupt requests are periodically serviced
DMA