Set MAC filter (expanded).
int32_t mac_async_set_filter_ex( struct mac_async_descriptor *const descr, uint8_t mac )
Set MAC filter. The Ethernet frames matching the filter, will be received.
Type: struct mac_async_descriptor Struct *const
Pointer to the HAL MAC descriptor
Type: uint8_t
MAC address
Type: int32_t
Operation status.
Success.