Send a command to stop an ADTC command on the selected slot.
bool mci_sync_adtc_stop( struct mci_sync_desc * mci, uint32_t cmd, uint32_t arg )
Type: uint32_t
Command definition
Type: uint32_t
Argument of the command
Type: bool
True if success, otherwise false