The bit masks are predefined in the device header file. For example, the bit mask for the ADPSIS bit is defined as below.
#define _ADCON2_ADPSIS_MASK 0x80
The naming convention adopted for the predefined bit masks in the header file is presented in Figure 2-2 with an example for the ADPSIS bit in the ADCON2 register.