This section covers considerations when updating a register bit field using various header file defines. The following bit field will be used as an example, where an update is needed, compared to the initialization configuration covered in 3.2. Register Initialization section.
1001
(previous
setting)0111
(new
setting)