The ADC can generate the following output
events:
- Result Ready (RESRDY): Generated
when the conversion is complete and the result is available.
- Window Monitor (WINMON): Generated
when the window monitor condition match.
Setting an Event Output bit in the Event
Control Register (EVCTRL.xxEO=1) enables the corresponding output event. Clearing this bit
disables the corresponding output event. Refer to the Event System chapter for
details on configuring the event system.
The peripheral can take the following
actions on an input event:
- Start conversion (START): Start a
conversion.
- Conversion flush (FLUSH): Flush the
conversion.
Setting an Event Input bit in the Event
Control register (EVCTRL.xxEI=1) enables the corresponding action on input event. Clearing
this bit disables the corresponding action on input event.
Note: If several events are connected to the
ADC, the enabled action will be taken on any of the incoming events. The events must be
correctly routed in the Event System.