In order to enable a peripheral that is
clocked by a Generic Clock, the following parts of the system needs to be configured:
- A running Clock Source.
- A clock from the Generic Clock Generator must be configured to use one of the running
Clock Sources, and the Generator must be enabled.
- The Generic Clock Multiplexer that provides the Generic Clock signal to the peripheral
must be configured to use a running Generic Clock Generator, and the Generic Clock must
be enabled.
- The user interface of the peripheral needs to be unmasked in the PM. If this is not
done the peripheral registers will read all 0’s and any writing attempts to the
peripheral will be discarded.