const char * strchrnul_P(const char *, int __val)
The strchrnul_P() function is like strchr_P() except that if c
is not found in s
, then it returns a pointer to the null byte at the end of s
, rather than NULL
. (Glibc, GNU extension.)
The strchrnul_P() function returns a pointer to the matched character, or a pointer to the null byte at the end of s
(i.e., s+strlen
(s)) if the character is not found.