char * strsep_P(char **__sp, const char *__delim)
The strsep_P() function locates, in the string referenced by *sp
, the first occurrence of any character in the string delim
(or the terminating '\0' character) and replaces it with a '\0'. The location of the next character after the delimiter character (or NULL
, if the end of the string was reached) is stored in *sp
. An ``empty'' field, i.e. one caused by two adjacent delimiter characters, can be detected by comparing the location referenced by the pointer returned in *sp
to '\0'. This function is similar to strsep() except that delim
is a pointer to a string in program space.
The strsep_P() function returns a pointer to the original value of *sp
. If *sp
is initially NULL
, strsep_P() returns NULL
.