char * strpbrk_P(const char *__s, const char *__accept) __ATTR_PURE__
The strpbrk_P() function locates the first occurrence in the string s
of any of the characters in the flash string accept
. This function is similar to strpbrk() except that accept
is a pointer to a string in program space.
The strpbrk_P() function returns a pointer to the character in s
that matches one of the characters in accept
, or NULL
if no such character is found. The terminating zero is not considered as a part of string: if one or both args are empty, the result will NULL
.