const char * strchr_P(const char *, int __val)
The strchr_P() function locates the first occurrence of val
(converted to a char) in the string pointed to by s
in program space. The terminating null character is considered to be part of the string.
The strchr_P() function is similar to strchr() except that s
is pointer to a string in program space.
The strchr_P() function returns a pointer to the matched character or NULL
if the character is not found.