int strncasecmp_P(const char *, const char *, size_t) __ATTR_PURE__
The strncasecmp_P() function is similar to strcasecmp_P(), except it only compares the first n
characters of s1
.
The strncasecmp_P() function returns an integer less than, equal to, or greater than zero if s1
(or the first n
bytes thereof) is found, respectively, to be less than, to match, or be greater than s2
. A consequence of the ordering used by strncasecmp_P() is that if s1
is an initial substring of s2
, then s1
is considered to be "less than" s2
.