int memcmp_PF(const void *, uint_farptr_t, size_t) __ATTR_PURE__
The memcmp_PF() function compares the first len
bytes of the memory areas s1
and flash s2
. The comparision is performed using unsigned char operations. It is an equivalent of memcmp_P() function, except that it is capable working on all FLASH including the exteded area above 64kB.
The memcmp_PF() function returns an integer less than, equal to, or greater than zero if the first len
bytes of s1
is found, respectively, to be less than, to match, or be greater than the first len
bytes of s2
.