GET

Used to get parameters on the tool.

For lists of valid get/set parameters, see SET/GET Parameters.

Table 1. Get
Field Size Description
GET (0x02) 1 byte Command ID
Version (0x00) 1 byte Command version
Get context 1 byte Context of the parameter to get
Address 1 byte Parameter ID/start address
Bytes 1 byte Number of bytes to read

Responses:

Note: Getting multiple parameters in one set call can only be done when all fields are in the same context.