To install the MPLAB® Code Configurator Plugin:
- 1.In MPLAB X IDE, select
Plugins from the Tools menu.
- 2.Select the Available
Plugins tab.
- 3.Check the box for the
MPLAB® Code Configurator v5, and click on
Install.
To install the library using Content Manager Tool (CMT):
- 1.Open MPLAB® Code Configurator v5 from the Tools/Embedded
menu.
- 2.Choose content type as Select MCC Classic from Content
Manager tab.
- 3.Under the "Optional" section, tick the box beside
CryptoAuthentication Library.
- 4.Click Finish from MCC Content Manager Wizard.
To switch the library version in an existing project:
- 1.Open MPLAB® Code the Tools/Embedded menu.
- 2.Click on Content Manager next to Device Resources
panel.
- 3.Expand Libraries component, look up CryptoAuthentication
Library and choose required version.
- 4.Click Apply.
To install the CryptoAuth Library offline:
- 1.Open the MPLAB Code Configurator page: https://www.microchip.com/mcc .
- 2.Select the MPLAB Code Configurator Downloads tab
- 3.Download the
CryptoAuthLibrary
(
CryptoAuthLibrary-2.0.2.mc3lib
).
- 4.In the MPLAB® X IDE, select Options from the Tools menu
- 5.Select MPLAB® Code Configurator v5.x tabfrom Plugins
option
- 6.Click on Install Library
- 7.Browse to the location where you saved the
CryptoAuthLibrary-2.0.2.mc3lib
, select and
click Open
- 8.Restart MPLAB® X IDE