This section lists all the FAQs related to the Libero SoC Design Suite installation.
The Libero SoC Design Suite service packs are add-on installations to the Libero SoC base version. Ensure that the base version is installed first and then update it with the service packs.
To use Libero SoC v11.7 SP1, Libero SoC v11.7 must be installed prior to SP1 installation.
Yes, you can install the Libero SoC Design Suite in any drive or folder. Ensure that the path used for each installation is unique. However, it is recommended to install the software inside a folder (on any drive) and not directly in a drive.
E:\ should not be directly used as the installation directory, rather E:\<some_folder>\ should be used as the installation path.
Run the Libero SoC Design Suite uninstaller from the Microsemi Libero start menu group or from the Windows control panel, add or remove software utility. If this does not work, and the Libero SoC software is not uninstalled, then contact Microsemi Customer Portal .
Yes, you can install different versions of Libero SoC software on the same computer. However, you must install each version in a different folder.
Contact Microsemi Customer Portal for debugging assistance on this issue. Following is the list of possible causes:
Yes, Microsemi provides a silent installation support. All installers (Libero, program Debug, and MSS) have provision to be installed silently. See Libero SoC Documentation for more information.
Yes, you must have administrative privileges to install, and to launch the Libero SoC Design Suite.