1.Create a new project in MPLAB® X IDE (for
ex: ATmega4808)
2.Open MCC by clicking Tools→ Embedded→
MPLAB® Code Configurator or click on the MCC icon
3.Navigate to Versions[MCC] → MPLAB® Code
Configurator (Plugin) → Libraries → Microchip Technology, Inc. → AVR-IoT Google Sensor
Node. Check the version of AVR IoT Google Sensor Node to ensure selection of library
version 2.0.1. If any other version is selected, double click on Library version
2.0.1.
4.In the Device Resources panel
navigate to Internet of Things → Examples → AVR-IoT Google Sensor Node
5.Double click on AVR-IoT Sensor Node to
add this to the Project Resources panel
6.In the Project Resources panel
navigate to Internet of Things → Examples → AVR-IoT Google Sensor Node
7.Select AVR-IoT Google Sensor Node
8.Google IoT Core
Configure the Project ID, Project
Region and Registry Id accordingly in Cloud Configuration.
The default values configured in
there is to get the sensor node connected to Microchip’s Sandbox account.
9.Click on the tooltip for more
information on each UI option.
10.Click Generate button
11.Connect the AVR-IoT WG Development Board
to the computer using a standard micro-USB cable
12.Build the firmware and program the
hardware.
13.Additional information is available in
AVR IoT WG User Guide (Documentation and Software
→ Documents).