The Revision mode of the Info
command reads back the silicon
revision of the ATECC608A-TNGTLS. This information is hard
coded into the device. This information may or may not be the same as what is read back
in the Revision bytes shown in the Configuration zone.
Opcode |
Mode |
Param |
Data |
Description |
---|---|---|---|---|
0x30 | 0x00 | 0x00 00 | — | Returns silicon revision |
Name | Response | Description |
---|---|---|
Response | 00 00 60 vv | Revision Info. 0x60 indicated ATECC608A-TNGTLS. vv is the most recent silicon version. |
0x00 0x00 0x60 0x02
. The response for the
ATECC608B devices will be 0x00 0x00 0x60 0x03
. The device revision is
the easiest way to determine which version of silicon you have. Over time the fourth
byte for the ATECC608B could change if additional silicon enhancements are
implemented.