Verify
CommandThe Verify
command takes an ECDSA [R,S] signature and
verifies that it is correctly generated given an input message digest and public key. In
all cases, the signature is an input to the command.
An optional MAC can be returned from the Verify
command to
defeat any man-in-the-middle attacks. If the verify calculation shows that the signature
is correctly generated from the input digest, then a MAC will be computed based on an
input nonce stored in TempKey and the value of the IO protection secret which is stored
in both the ATECC608A-TNGTLS and the host MCU. MAC outputs
can only be generated in External and Stored modes. The IO protection function must be
enabled for MAC computation.