A fixed nonce is passed to the device and stored in one of the internal buffers. The
size of the nonce may be either 32 or 64 bytes. The TempKey.SourceFlag is always set to
input after this command is run. This mode of the Nonce
command does
not run a SHA256 calculation or generate a random number.
Opcode | Mode | Param2 | Data | Description |
---|---|---|---|---|
0x16 |
0x03 |
0x00 | 32 bytes |
|
0x23 |
0x00 | 64 bytes |
|
Name | Size | Description |
---|---|---|
Response | 1 byte | 0x00 if the command is completed successfully. Otherwise an error code is received. |
1
’ upon successful command completion, indicating nonce
value was fixed input value.1
’, indicating the value is valid for other use.