The Flash is divided into a set of pages. A page is the basic unit addressed when programming the Flash. It is only possible to write or erase a whole page at a time. One page consists of several words.
The Flash can be divided into three sections in blocks of 256 bytes for different security. The three different sections are BOOT, Application Code (APPCODE), and Application Data (APPDATA).
The sizes of these sections are set by the Boot Section End (FUSE.BOOTEND) fuse and the Application Code Section End (FUSE.APPEND) fuse.
The fuses select the section sizes in blocks of 256 bytes. The BOOT section stretches from the start of the Flash until BOOTEND. The APPCODE section runs from BOOTEND until APPEND, and the remaining area is the APPDATA section.
BOOTEND | APPEND | BOOT Section | APPCODE Section | APPDATA Section |
---|---|---|---|---|
0 |
— |
0 to FLASHEND |
— |
— |
> 0 |
0 |
0 to 256*BOOTEND |
256*BOOTEND to FLASHEND |
— |
> 0 |
≤ BOOTEND |
0 to 256*BOOTEND |
— |
256*BOOTEND to FLASHEND |
> 0 |
> BOOTEND |
0 to 256*BOOTEND |
256*BOOTEND to 256*APPEND |
256*APPEND to FLASHEND |
If BOOTEND is written to ‘0
’, the entire Flash is regarded as the BOOT
section. If APPEND is written to ‘0
’ and BOOTEND >
0
, the APPCODE section runs from BOOTEND to the end of Flash (no APPDATA
section). When APPEND ≤
BOOTEND, the APPCODE section is removed, and
the APPDATA runs from BOOTEND to the end of Flash. When APPEND >
BOOTEND, the APPCODE section spreads from BOOTEND until APPEND. The remaining area is
the APPDATA section.
If there is no boot loader software, it is recommended to use the BOOT section for Application Code.
If FUSE.BOOTEND is written to 0x04
and FUSE.APPEND is written to
0x08
, the first 4*256 bytes will be BOOT, the next 4*256 bytes will
be APPCODE, and the remaining Flash will be APPDATA.
Additional to the inter-section write protection, the NVMCTRL provides a security mechanism to avoid unwanted access to the Flash memory sections. Even if the CPU can never write to the BOOT section, a Boot Section Lock (BOOTLOCK) bit in the Control B (NVMCTRL.CTRLB) register is provided to prevent the read and execution of code from the BOOT section. This bit can be set only from the code executed in the BOOT section and has effect only when leaving the BOOT section.
The Application Code Section Write Protection (APCWP) bit in the Control B (NVMCTRL.CTRLB) register can be set to prevent further updates of the APPCODE section.