The default value given in this fuse description is the
factory-programmed value and should not be mistaken for the Reset
value.
Application Code Section End
These bits set the
end of the application code section in blocks of 256
bytes. The end of the application code section should be set as the BOOT size plus
application code size. The remaining Flash will be application data. A value of 0x00
defines the Flash from BOOTEND*256 to the end of Flash as the application code
section. When FUSE.BOOTEND is 0x00
, the entire Flash is the BOOT section.