The Single-Shot mode can be used to generate a pulse with a duration defined by the Compare (TCBn.CCMP) register every time a rising or falling edge is observed on a connected event channel.
When the counter is stopped, the output pin is driven to low. If an event is
detected on the connected event channel, the timer will reset and start
counting from BOTTOM to TOP while driving its output high. The RUN bit in
the Status (TCBn.STATUS) register can be read to see if the counter is
counting or not. When the Counter register reaches the CCMP register value,
the counter will stop, and the output pin will go low for at least one
prescaler cycle. A new event arriving during this time will be ignored.
There is a two clock-cycle delay from when the event is received until the
output is set high. When the EDGE bit of the TCB.EVCTRL register is written
to ‘1
’, any edge can trigger the start of the counter. If
the EDGE bit is ‘0
’, only positive edges trigger the
start.
The counter will start counting as soon as the module is enabled, even without
triggering an event. This is prevented by writing TOP to the Counter
register. Similar behavior is seen if the Event Edge (EDGE) bit in the Event
Control (TCBn.EVCTRL) register is ‘1
’ while the module is
enabled. Writing TOP to the Counter register prevents this as well.
If the Event Asynchronous (ASYNC) bit in the Control B (TCBn.CTRLB) register is
written to ‘1
’, the timer will react asynchronously to an
incoming event. An edge on the event will immediately cause the output
signal to be set. The counter will still start counting two clock cycles
after the event is received.
This mode requires TCB to be configured as an event user and is explained in the Events section.