A clarification has been made for the Fuse Description section concerning the fuse default values. The data sheet refers to these values as reset values when they should have been referred to as factory-programmed values. Also, they are given in both hexadecimal and binary values, which contradicts each other.
The following sentence has been added to each sub-section of the Fuse Description section.
The default value given in this fuse description is the factory-programmed value and should not be mistaken for the Reset value.
The table below lists the reset values given by the data sheet and the actual factory-programmed default values.
Fuse | Stated Reset Value in Data Sheet | Actual Factory Default on Device | ||
---|---|---|---|---|
Hexadecimal | Binary | Hexadecimal | Binary | |
WDTCFG | - | `b00000000 |
0x00 |
`b00000000 |
BODCFG | - | `b00000000 |
0x00 |
`b00000000 |
OSCCFG | - | `b0XXXXX10 |
0x01 |
`b00000001 |
TCD0CFG | - | `b00000000 |
0x00 |
`b00000000 |
SYSCFG0 | 0xC4 |
`b11X101X0 |
0xF6 |
`b11110110 |
SYSCFG1 | - | `bXXXXX111 |
0x07 |
`b00000111 |
APPEND | - | `b00000000 |
0x00 |
`b00000000 |
BOOTEND | - | `b00000000 |
0x00 |
`b00000000 |
LOCKBIT | - | `b00000000 |
0xC5 |
`b11000101 |