To generate this project using MPLAB Code Configurator (MCC), follow the next steps:
- 1.Create a new MPLAB X IDE project for
PIC18F47Q10.
- 2.Open MCC from the toolbar (more
information about how to install the MCC plug-in can be found here).
- 3.Go to Project Resources →
System → System Module and make the following configurations:
- Oscillator Select:
HFINTOSC
- HF Internal Clock: 1 MHz
- Clock Divider: 1
- In the Watchdog Timer Enable
field in the WWDT tab, WDT Disabled has to be selected
- In the Programming
tab, Low-Voltage Programming Enable has to be checked
- 4.From the Device Resources window, add
TMR0 and make the following configurations:
Timer0
Configuration:
- Enable Timer: checked
- Timer Clock tab
- Clock Source:
LFINTOSC
- Clock Prescaler:
1:1
- Postscaler: 1:1
- Timer mode:
8-bit
- Enable
Synchronization: unchecked
- Timer period: 4 ms
- Enable Timer Interrupt:
unchecked
- 5. Open Pin Manager → Grid
View window and select UQFN40 in the MCU package field and
make the following pin configuration:
- Set Port C pin 2 (RE0) as
output
Figure 1. Pin Mapping
- 6.Click Generate in the
Project Resources tab.