The following schematic checklist is only necessary if the application is using one or more of the external analog references. If the internal references are used instead, the circuits in the following two figures are not necessary.
Signal Name | Recommended Pin Connection | Description |
---|---|---|
VREFx | 1.0V to (VDDANA - 0.6V) for ADC 1.0V to (VDDANA - 0.15V) for DAC Decoupling/filtering capacitors 100nF(1)(2) and 4.7µF(1) | External reference VREFx for the analog port |
GND | Ground |
1. These values are only given as a typical example.
2. Decoupling capacitor should be placed close to the device for each supply pin pair in the signal group.