Each individual operational amplifier is configured by its respective Operational Amplifier Control x register (OPAMPCTRLx). These settings must be configured before the amplifier is started.
- Select the positive input in
OPAMPCTRLx.MUXPOS
- Select the negative input in
OPAMPCTRLx.MUXNEG
- Select RES1EN if resistor ladder is
used
- Select the input for the resistor
ladder in OPAMPCTRLx.RES1MUX
- Select the potentiometer selection of
the resistor ladder in OPAMPCTRLx.POTMUX
- Select the VCC input for the resistor
ladder in OPAMPCTRLx.RES2VCC
- Connect the operational amplifier
output to the resistor ladder using OPAMPCTRLx.RES2OUT
- Select the trade-off between speed and
energy consumption in OPAMPCTRLx.BIAS
- Select RES3TAP as positive input for the OPAMP2 and connect the resistor ladder to
OA0OUT by setting the RESCTRL.RES2OUT bit only if OPAMPs are configured as a High Gain
Instrumentation Amplifier