Important: For SAM
L11 Non-Secure accesses, read and
write accesses (RW*) are allowed only if the security attribution for the corresponding
I/O pin is set as Non-Secured in the NONSEC register.
This register allows the
user to toggle the direction of one or more I/O pins, without doing a read-modify-write
operation. Changes in this register will also be reflected in the Data Direction (DIR),
Data Direction Set (DIRSET) and Data Direction Clear (DIRCLR) registers.
Tip: The I/O pins are
assembled in pin groups (”PORT groups”) with up to 32 pins. Group 0 consists of the
PA pins, group 1 is for the PB pins, etc. Each pin group has its own PORT registers,
with a 0x80 address spacing. For example, the register address offset for the Data
Direction (DIR) register for group 0 (PA00 to PA31) is 0x00, and the register
address offset for the DIR register for group 1 (PB00 to PB31) is 0x80.
|
0x0C |
32 |
PAC Write-Protection, Mix-Secure |
0x00000000 |
|
Port Data Direction Toggle
Writing
'0' to a bit has no effect.
Writing '1' to a bit will toggle the corresponding bit
in the DIR register, which reverses the direction of the I/O pin.
Value | Description |
---|
0 |
The corresponding I/O pin in the PORT
group will keep its configuration. |
1 |
The direction of the corresponding
I/O pin is toggled. |