In this step, HDL is verified for timing closure. In libero.tcl
, use the
following command to run Timing Verification.
run_tool -name {VERIFYTIMING}
Use this command with the catch statement as shown in the following snippet.
if {[catch {run_tool -name {VERIFYTIMING} }] } {
puts "VERIFYTIMING FAILED \n"
} else {
puts "VERIFYTIMING PASSED \n"
}
For more information about adding Verify Timing parameters, see Tcl Commands Reference Guide for Libero SoC Design Suite.