In this step, HDL is placed and routed according to constraint files. In
libero.tcl
, use the following command to run Place and Route.
run_tool -name {PLACEROUTE}
Use this command with the catch
statement as shown in the following
snippet.
if {[catch {run_tool -name {PLACEROUTE} }] } {
puts "PLACEROUTE FAILED \n"
} else {
puts "PLACEROUTE PASSED \n"
}
For more information about adding Place and Route parameters, see Tcl Commands Reference Guide for Libero SoC Design Suite.