Right-click the net and select Go to Net Driver to trace the net to the driver. This feature allows you to easily retrieve the driver of a net. When the net driver is retrieved, the display is centered on the net driver.
If the Do Selection Locally option is turned ON, the trace will stop on the current level of hierarchy. If the Do Selection Locally option is turned OFF, the trace crosses hierarchy boundaries until the instance driving the net is reached. The instance (net driver) is selected in the view.