To go up one level of hierarchy in the Netlist Viewer:
- 1.Click to select an instance and right-click
Pop Up current level <instance_name>.
- 2.Click the Pop icon on the Toolbar or right-click
and select Pop Instance <instance_name> or double-click an empty
area in the canvas to move up one level of hierarchy.
Note: The right-mouse click pop instance menu item is not available at the top of the design
hierarchy.
Figure 1. Pop Up Instance