The Address Header following a Start condition (but not a Restart condition) is subject to
arbitration, meaning multiple devices on the bus may attempt to drive an address on the
bus using SDA lines. The Controller may drive the SDA line to transmit the address of a
device it intends to communicate with. The Target may drive the SDA line to transmit its
own address while requesting for Hot-Join or In-Band Interrupt. The Address Header Arbitration process is described in Figure 1. The Target loses Address Arbitration when
it releases the SDA line to transmit a ‘1
’, but another device on the
bus drives it low to transmit a ‘0
’.