The I3C Target module can be connected to a Legacy I2C Bus or an I3C Bus. The module can act as an I2C Target using static address in the I3CxSADR register until it is assigned a dynamic address by an I3C Controller.
The Target can participate in the following types of transactions on the bus:
The I3C Target module follows the typical SDR bus communication flow as outlined below in Figure 1.