VDDIOx supply voltage is available as an internal input channel to the ADC.
The voltage is divided by ten to allow the use of any internal ADC reference. To measure
VDDIOx/10, the user is recommended to follow these steps:
- 1.Configure the voltage reference for
the ADC.
- 2.Select VDDIOx/10 as the
positive input to the ADC.
- 3.Run a single-ended ADC
conversion.
- 4.Calculate the voltage using the
following equation:
VDDIOx=ADC Result×VREF×10ADC Resolution