Some peripherals that can operate in High-Power Sleep mode (VREGPM =
‘b00
) will not operate as intended in the Low-Power Sleep modes (VREGPM
= ‘b01
and ‘b11
). The Low-Power Sleep modes are intended
for use with the following peripherals:
It is the responsibility of the end user to determine what is acceptable for their application when setting the VREGPM settings to ensure correct operation in Sleep.