The Controller uses the Direct SETNEWDA CCC to set a new Dynamic Address for the Target when it already has a Dynamic Address assigned. The frame format is shown in Figure 1. The Target’s new Dynamic Address is the first 7 bits of the 9-bit Dynamic Address field. This new address is stored in I3CxDADR register. Refer to Changing Dynamic Address for more details.