The following section describes the sequence of events that occur when the
module is receiving data in 7-bit Addressing mode:
- 1.The host issues a Start condition.
Once the Start is detected, client hardware sets the Start Condition Interrupt Flag
(SCIF) bit. If the Start Condition Interrupt Enable (SCIE) bit is also set, the generic I2CxIF bit is also
set.
- 2.Host hardware transmits the address
high byte with the R/W bit clear
(R/W =
0
).
- 3.The received high address byte is
compared to the values in the I2CxADR registers. If the client is configured in
10-bit Addressing mode (no masking), the received high address byte is compared to
the values in the I2CxADR1 and I2CxADR3
registers. If the client is configured in 10-bit Addressing with Masking mode, the
received high address byte is compared to the masked value in the I2CxADR1
register.
If a high address match occurs:
- The
R/W bit value is copied to the Read Information
(R) bit by module hardware.
- The Data (D) bit is cleared (D =
0
) by hardware, indicating the
last received byte was an address.
- The Address Interrupt Flag
(ADRIF) bit is set (ADRIF =
1
). It
is important to note that regardless of whether the Address Interrupt and
Hold Enable (ADRIE) bit is set, clock stretching does not occur
when the R/W bit is clear in 10-bit Addressing
modes.
- The matching address is
loaded into either the I2CxADB1 register or into the I2CxRXB register as determined by the Address Buffer Disable
(ABD) bit. When ABD is clear (ABD =
0
), the matching address is copied to I2CxADB1. When
ABD is set (ABD = 1
), the matching address is copied to
I2CxRXB, which also sets the Receive Buffer Full Status (RXBF) bit and the I2C Receive Interrupt Flag
(I2CxRXIF) bit.
If no address match occurs, the module remains Idle.
- 4.The host device transmits the 9th
clock pulse, and client hardware transfers the value of the ACKDT bit onto the SDA line. If there are pending errors,
such as a receive buffer overflow (RXO =
1
), client hardware generates a NACK
and the module goes Idle.
- 5.The host device transmits the low
address byte. If the client is configured in 10-bit Addressing mode (no masking),
the received low address byte is compared to the values in I2CxADR0
and I2CxADR2. In 10-bit Addressing with Masking mode, the received low
address byte is compared to the masked value of I2CxADR0.
If a match
occurs:
- The Client Mode Active (SMA) bit is set by module hardware.
- ADRIF is set. If ADRIE is set, and the Clock Stretching Disable
(CSD) bit is clear, hardware sets the Client Clock
Stretching (CSTR) bit and the generic I2CxIF bit. This allows
time for the client to read either I2CxADB0 or I2CxRXB and selectively ACK/NACK based
on the received address. When the client has finished processing the
address, software must clear CSTR to resume operation.
- The matching received address
is loaded into either the I2CxADB0 register or into the I2CxRXB register as determined by the ABD bit. When ABD is clear (ABD =
0
), the matching address is copied to I2CxADB0. When
ABD is set (ABD = 1
), the matching address is copied to
I2CxRXB, which also sets the RXBF and the I2CxRXIF bits. I2CxRXIF is a read-only
bit, and must be cleared by either reading I2CxRXB or by setting the Clear
Buffer (CLRBF) bit (CLRBF = 1
).
If no match occurs, the module goes Idle.
- 6.The host device transmits the 9th
clock pulse, and client hardware transfers the value of the ACKDT bit onto the SDA line. If there are pending errors,
such as a receive buffer overflow (RXO =
1
), client hardware generates a NACK
and the module goes Idle.
- 7.After the 9th falling edge of SCL,
the Acknowledge Status Time Interrupt Flag (ACKTIF) bit is set. If the Acknowledge Time Interrupt and
Hold Enable (ACKTIE) bit is also set, the generic I2CxIF is set, and if
client hardware generated an ACK, the CSTR bit is also set and the clock is stretched (when CSD =
0
). If a NACK was generated, the
CSTR bit remains unchanged. Once completed, software must
clear CSTR and ACKTIF to release the clock and resume operation.
- 8.If client hardware generated a NACK,
host hardware generates a Stop condition, the Stop Condition Interrupt Flag (PCIF) is set when client hardware detects the Stop
condition, and the client goes Idle. If an ACK was
generated, host hardware transmits the first seven bits of the 8-bit data byte.
- 9.If data remains in I2CxRXB
(RXBF =
1
and I2CxRXIF =
1
) when the first seven bits of the new byte are received by the
shift register, CSTR is set, and if CSD is clear, the clock is stretched after the 7th falling
edge of SCL. This allows time for the client to read I2CxRXB, which clears RXBF and I2CxRXIF, and prevents a receive buffer overflow.
Once I2CxRXB has been read, RXBF and I2CxRXIF are cleared, and hardware releases
SCL.
- 10.Host hardware transmits the 8th bit
of the current data byte into the client receive shift register. Client hardware
then transfers the complete byte into I2CxRXB on
the 8th falling edge of SCL, and sets the following bits:
- I2CxRXIF
- I2CxIF
- Data Write Interrupt Flag
(WRIF)
- Data (D)
- RXBF
I2CxCNT is decremented by one. If the Data Write Interrupt and Hold
Enable (
WRIE) bit is set (WRIE =
1
), hardware
sets
CSTR (when
CSD =
0
) and stretches the clock,
allowing time for client software to read
I2CxRXB and determine the state of the
ACKDT bit that is transmitted back to the host. Once
the client determines the Acknowledgement response, software clears CSTR to
allow further communication.
- 11.Upon the 9th falling edge of SCL, the
ACKTIF bit is set. If ACKTIE is also set, the generic I2CxIF is set, and if CSD is clear, client hardware sets CSTR and stretches the clock. This allows time for software
to read I2CxRXB. Once complete, software must clear both CSTR and ACKTIF to
release the clock and continue communication.
- 12.Repeat steps 8–11 until the host has
transmitted all the data (I2CxCNT =
0
), or until the host issues a
Stop or Restart condition.
Figure 1. 10-Bit Client Mode
Reception