Initialize the MVIO in Dual Supply configuration by following these steps:
- 1.Set the VDDIOxMD bit in the
appropriate configuration register to select the Dual Supply mode.
- 2.Optional: Enable the
VDDIOx Interrupt by setting the VDDIOxIE bit in the appropriate PIEx
register.
- 3.Read the VDDIOxRDY bit in the MVIOSTAT status register to check if the
VDDIOx voltage is within the acceptable range of operation.
- 4.Configure and use the PORT pins
powered by VDDIOx as usual.
If the VDDIOxMD configuration bit is programmed to the Single Supply mode, the VDDIOxRDY
status bit is read as ‘0
’, and the VDDIOxIF Interrupt flag in the PIRx
register is read as ‘0
’.