Target Reset Pattern Received Without Any RSTACT CCC

If the Target has not been configured by the RSTACT CCC yet or if the Target was unable to recognize the RSTACT CCC sent by the Controller (dysfunctional target), the Target will still set the RSTDET bit and the I3CxRIF system level interrupt flag. To be compliant with the I3C protocol, it is recommended the user software behave as follows:
Important: Performing the appropriate level of software Reset of the I3C Target module or the entire device is left up to the discretion of the user and the specific application.