End of a CCC Command

A Broadcast CCC frame ends when either one of the following Bus conditions occur after a command or data:

A Direct CCC frame ends when either one of the following bus conditions occur after a command or data:

These conditions are illustrated in Figure 1 and Figure 2.

In addition to the above-mentioned conditions, the Controller can terminate any CCC prematurely at any time by issuing a Stop condition. The Target handles this premature termination, and responds by setting an appropriate Bus error condition.