The XMEGA can be programmed and debugged by connecting an external programming/debugging tool to the PDI header shown in Figure 1.
The gray XMEGA PDI adapter must be used on the Atmel AVR JTAGICE mkII probe when connecting to the XMEGA-E5 Xplained board.
The green standoff adaptor nr.3 (ref.A08-0254) has to be used on the Atmel AVR ONE! probe when connecting to the XMEGA-E5 Xplained board.
Pin on programming header | PDI |
---|---|
1 | DATA |
2 | VCC |
3 | - |
4 | - |
5 | CLK |
6 | GND |