This section walks
you
through the basic steps for getting up and running with simple conversion
and experimenting with MUX settings for ATtiny88
devices.
The necessary registers are described along with relevant bit settings.
General Instructions
to Test the Code on STK600
- Place the
ATtiny88 device onto the STK®600 using the specific routing card and/or
socket card
- Try accessing the
device from the menu Tools → Device Programming in Atmel
Studio
- The voltage from
AREF1 can be used as input to the ADC. Adjust the AREF1
voltage via the menu Tools → Device Programming → Board
settings in Atmel Studio.
- Connect AREF1 on
the STK600 to the ADC input channel ADC0 (PC0) used in the
examples
- On the STK600,
connect PB0 to LED0. Also, connect PB1 to LED1. These pins
are used in the following examples to give visual
indication. Also connect PB5 to the SW0 switch.