Test Steps
- 1.Build the project and load the
hex file into the device.
- 2.Make the arrangements on STK600
as described in the beginning of the section.
- 3.Adjust the voltage applied to PC0
and check whether the LED indication is updated depending on the voltage.
- 4.If the voltage on PC0 is higher
than ~0.5V, the LED0 connected to PB0 will remain OFF. Otherwise the LED0
remains ON. The LED1 connected to PB1 is always twinkling, indicating the
project is running.