Best Practices for Improving ADC Performance

The performance of an ADC depends on the quality of the input signals and power supplies. The following points should be taken into consideration for improving the accuracy of ADC measurements:
Note: Some points mentioned below might not be applicable for all tinyAVRs based on their feature set. Refer to the device data sheet for further information.